2020-10-23 1:44 PM
Hi,
I see there are different states for SPI transfer/Receive.
There are 4 different status when we use HAL_SPI_Transmit_Receive_DMA()
What is the next step if we receive the status as HAL_BUSY, HAL_ERROR, HAL_TIMEOUT.
Can you please help me to get some state machine?
2020-10-23 2:02 PM
If it's busy, wait until it's done to use it.
If there's an error, figure out the source of the error and fix it. A few things can trigger this, see the source code for HAL_SPI_TransmitReceive_DMA.
I don't see how a timeout is possible.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.