2025-12-28 10:35 AM
Ambiente
Sistema operativo Mac Tahoe 26.2 (25C56)
Apple Silicon M4
STM32CubeIDE 2.0.0 (x86_64, ejecutándose bajo Rosetta 2)
Asunto
STM32CubeIDE se inicia correctamente, pero la selección de texto no se representa visualmente en ninguna parte del IDE (editor, consola, vistas).
La selección del mouse y del teclado no muestra ningún resaltado.
Copiar/pegar funciona normalmente , lo que indica que la selección existe internamente pero no se muestra.
La selección de texto funciona correctamente en otras aplicaciones de macOS.
Pasos para reproducir
1. Inicie STM32CubeIDE en Rosetta:
arch -x86_64 /Aplicaciones/ST/STM32CubeIDE.app/Contenidos/MacOS/STM32CubeIDE
2.Abra cualquier archivo fuente.
3.Intenta seleccionar texto.
Solución de problemas realizados
Instalación de Rosetta 2 verificada.
Restablecer preferencias y espacio de trabajo.
Espacio de trabajo limpio probado.
Deshabilitado el renderizado SWT Metal/gestos a través de opciones .ini.
El problema persiste.
2026-01-11 8:08 AM
I can advise to do a rework. its easy and solves issues on 26.2 Tahoe for 1.19. The link is 1 post above
2026-01-12 7:33 AM
Hello @FOFI
Our development team remains committed to customers and collaborators satisfaction and is engaged in aligning the STM32CubeIDE with macOS Tahoe 26.2.
We will share further information as it becomes available.
2026-01-16 6:33 AM
Thanks, I assume this does not work for version 2.0? I have tried it twice and upon start using clean I get an error log containing
Caused by: java.lang.ClassNotFoundException: An error occurred while automatically activating bundle org.eclipse.ui.workbench (388).
2026-01-16 7:13 AM
Hello,
I didn't check 2.0 but other report its working. I had errors lunching as well. how do you open the LIST file ? with Text.edit ? if so - check the pasted name with the file name. For some reaspon it can autocorrect : " , " to " _ " or opposite
2026-01-16 7:17 AM
I already confirmed that wasn’t the issue. I tried it a second time using VS Code, since I know how unpredictable TextEdit can be. I’ve given up for now and am currently downgrading my machine to Sequoia, as I’m also not satisfied with the current design choice.
2026-01-16 7:27 AM
Sorry to hear that. On a side note, can you confirm if you can flash your MCU with V3minie dongle on Tahoe ? (If you use V3minie of course)
2026-01-16 7:27 AM
I do not have the V3minie.
2026-02-27 7:45 AM
Still looking for an update, patch or workaround.
2026-02-27 10:14 AM
The fix exist. Need to manually patch Eclipse files.
2026-04-16 7:51 AM
I just ran into the same problem. MacOS was updated and now can't see selected text.
IDE 2.1.1
MacOS 26.4.1
Apple M4 Pro
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.