cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to Import example .

shreya_awati
Associate III

 

shreya_awati_1-1779432370928.png

shreya_awati_2-1779432566427.png

 

i am installed cube-MX for linux laptop version (6.17.0) and cube-IDE is (Version: 2.1.1) .
For MX it shows option only generlic linux  so it is correct for linux laptop ? and for IDE is debian is fine . 

I refer you tube sessions for Example import in that STM32IDE option availbale as toolchain but in my system sometimes not shows . Can you please give me exact steps how can i use Mx with IDE in detail steps for import examples given by stm32 also how can i create and import new example also . 

 

Also i have board STM32-NUCLEO-F746ZG when i import example in MX sometimes board is not visible .

For toolchain selection below options are availble in that STM32IDE is invisible .

shreya_awati_3-1779432973798.png

 



 

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @@shreya_awati 

Let me thank you for posting and welcome to the ST Community.

I recommend that you take a look at this Knowledge Article.

It mentions how to create a project with STM32CubeMX Standalone and import it on STM32CubeIDE.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This is for create new project and import that i did successfully . but i am facing issue in import multiple examples provided by stm32 for reference . you can check my shared above query,