2024-08-03 11:23 AM
Hello,
I updated to Mac15 (MacOS Sonoma Public Beta), which was probably a mistake. Now I get an error from STMCubeIDE when I try to run indicating "ST-Link Server is required to launch the debug session" and to Please download it on www.st.com.
I figured something changed in the OS that no longer makes the ST-Link Server run any more.
However when I try to download it, I get essentially a broken link, or at least it simply wont download. Even worse, the web page with Safari seems entirely broken and I cant even get a download to start after accepting the license, but with FireFox I get further, I get but still wont download and the link seems broke.
I can still flash using the STM32CubeProgrammer fortunately (using 2.13.1).
Can anyone tell me how to download this ST-Link Server? Or if there is an issue with the last MacOS and this and there is no fix?
Solved! Go to Solution.
2024-11-28 11:51 AM
thanks so much.
2024-12-02 9:41 AM
I can confirm that it DOES work with MacOS 15.1.1 and CubeIDE 1.17.0.
Updating from 1.16.x was a complete bust, there was an issue with the popup dealing with trusting various packages not having any content, then having to chase it across various monitors, then it wouldn't take clicks, so I just did a clean install of 1.17.0 and it just worked.
2024-12-10 2:44 PM
Thanks Rohdea, your sudo fix worked for me.
Does anyone know if there is now a 'proper' solution to this issue?
I'm using Sequoia 15.1.1. I repeatedly got "ST-Link Server is required to launch the debug session" until I tried Rohdea's fix.
2024-12-10 10:52 PM
Upgrading to STM32CubeIDE 1.17.0 (on MacOS Sequoia 15.1.1) solved the issue for me.
2024-12-12 2:52 AM
Thanks so much @fsteiner , worked for me too!
2025-02-11 4:13 AM
See replies in https://community.st.com/t5/stm32-mcus-boards-and-hardware/st-link-server-is-required-error-after-macos-update/td-p/719546 that points to https://stackoverflow.com/questions/78996974/stm32cubeide-debugger-no-longer-works-in-macos-15-0-sequoia
1) if `locate stink-server` does not work then use `where stlink-server`
2) mine stink-server is found at /usr/local/bin. This path is included in /etc/paths (global OS settings) and also seen in `echo $PATH`. So, starting IDE from CLI also helps to use ST-Link even without superuser rights and STM32CubeProgrammer works as it was before macOS 15 upgrade
3) if you ever started STM32CudeIDE under superuser account then your workspace files can be spoiled with superuser permissions. IDE could complain about impossibility to save some settings. But it looks like it can fix itself.
4) Running STM32CubeIDE from application shortcut still does not work.
2025-02-24 8:22 AM - edited 2025-02-24 8:47 AM
Hello,
Issue come back in MacOS 15.3.1 and launch in sudo doesn't fix. Please help
2025-11-28 7:04 AM
any fix?
2025-11-28 9:05 AM
@tbwentmia This post has been marked as solved and the solution is highlighted.
If you have an issue, consider creating a thread with the relevant information and someone may take a look.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.