2023-01-12 2:33 AM
Hi,
I need to debug several axf files. In 'debug configurations' -> Startup, I added the axf files that contain debug information. It works fine but only up to 4 files. If I load 5'th file the debugger presents the message:
"Failed to insert all hardware breakpoints:
You may have requested too many hardware breakpoints/watchpoints"
Then debug session is terminated.
Is there a way to overcome this problem?
Thank you
2023-01-12 11:48 AM
Have seen this error if I tried to set more breakpoints than supported by the ARM debug peripheral of the core. Double-check your breakpoints set and alos check if the debugger startup is configured to auto-insert a breakpoint at main (which consumes one additional breakpoint).
hth
KnarfB
2023-01-16 3:19 AM
Hi,
Thanks for response.
This issue occurs also when "insert a breakpoint at main" is unchecked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.