STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32N6 Index Problem

Hello,I am working on USB Device VCP project but I have problem about defines,index,etc. As you can see below that I have definition of "STM32N655xx" but I can not include "stm32n655xx.h".I tried Index, Rebuild step but it did not fix. On the other h...

BKaya_0-1750412741674.png BKaya_1-1750412775627.png BKaya_0-1750416360701.png
B.Kaya by Associate III
  • 1101 Views
  • 2 replies
  • 0 kudos

Resolved! [Nucleo-N657X0-Q ]How to use swv printf in Keil arm mdk 5.39

I would like to use SWV for debugging on the Nucleo-N657X0-Q board.I first enabled SWV debugging and also change the CPU clock to 400 MHz.   Then, I added some code to main.c (as reference here ).At the same time, I also set the core clock to 50 MHz ...

image.png bioak_0-1750155820298.png bioak_3-1750157556553.png bioak_1-1750156771078.png
bioak by Associate II
  • 1339 Views
  • 2 replies
  • 2 kudos

cube ide strange breakpoint behaviour

Using cube IDE to debug my application i've witnessed breakpoints behaving unpredictably: sometimes they appear on their own in breakpoint list view while not present in the file editing view; other times the breakpoints i've just placed and just use...

Resolved! How to clone/copy an STMCube Example project

Hello,I'm new to STM32Cube-IDE (and Eclipse). Normally I use the ARM-gcc toolchain and do assembly coding.I managed to create a New STM Project by using the Example Selector tab in the Target Selection window.In this case it was the BSP Example for t...

Screenshot 2024-08-11 at 02.02.14.png
cc2 by Associate
  • 2869 Views
  • 3 replies
  • 1 kudos

Live Expressions showing wrong values

I am using CubeIDE version 1.11.0 for a STM32F411RC project. After i've changed boards (between two equal custom boards), my live expressions started showing wrong values. The values are only wrong in the live expression, because if I halt the progra...

THML by Associate II
  • 6822 Views
  • 9 replies
  • 5 kudos

Resolved! Unable to install STM32CubeIDE plugin from jar file

I bought an analysis program from a company and they gave me a plugin .jar file to install the analysis program in IDEs. When I put this plugin .jar file in a folder called dropins in the Code Composer Studio IDE folder, it works directly. But in STM...

dikene by Associate II
  • 1114 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.