STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! New errors when compiling assembly only project

Hello,we're maintaining assembly projects to teach baremetal assembly programming on STM32H750 board.Project used to compile without and warnings, but lately we're getting new errors.Project is stripped down to bare assembly and probably something is...

bully by Senior
  • 2521 Views
  • 3 replies
  • 1 kudos

Unable to debug using OpenOCD under STM32CubeIDE

I am attempting to debug code on a Necleo-U385RG-Q board using STM32CubeIDE V1.18.1 under Windows 11. I beleive that under \plugins\com.st.stm32cube.ide.mcu.externaltools.openocd.win32_2.4.100.202501161620\tools there should be a scripts directory th...

Validation on target falling on F4 Discovery

Hi, I'im running X-CUBE-AI with STM32Cube IDE on a F407 Discovery. When I try to perform validatation on target, I get the following error during building stage :  Building project /opt/st/stm32cubeide_1.18.1/plugins/com.st.stm32cube.ide.mcu.external...

PauloP by Associate
  • 782 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G4: trigger SPI DMA through GPIO EXTI event?

Hi, I want to get data from an ADC connected externally through SPI DMA whenever data ready pin is set. I want to do it without any interrupt handler, since our firmware have already loaded with other stuffs. I have tried the synchronisation of SPI D...

BrindhaP by Associate II
  • 4705 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.