2024-08-13 7:48 AM
Hello,
I'm new to STM32Cube-IDE (and Eclipse). Normally I use the ARM-gcc toolchain and do assembly coding.
I managed to create a New STM Project by using the Example Selector tab in the Target Selection window.
In this case it was the BSP Example for the B-U585I-IOT02A Discovery Kit (with the STM32U585 chip).
After modifying the code in accordance with how-to-use-semihosting-with-stm32cubeide the code runs OK.
Now I would like to COPY the Project and edit that.
From the multiple "how to clone a project" threads it appears that this is not trivial. (?) One of the threads I read was from 2022 and IDE version 1.8. It seemed that multiple otherwise experienced developers found it odd that this wasn't a straightforward task.
Manually copying and search/replace seems very odd and error-prone.
Has there been any progress on automating this?
In my case there aren't even any .ioc or .project files.
As expected, the following don't work:
Simply copying the Project's directory (in the Workspace directory)
Using File->Open Projects From File System...
For now, I have created a new workspace and reimported the STM32Cube Example. But now I have to redo the edits and modifications to get the semihosting working again...
As an aside, at the end of the Example import I get the following (not very informative) error (which I ignore).
Solved! Go to Solution.
2024-08-13 11:19 AM - edited 2024-08-13 11:20 AM
This is very fast and straighforward:
1. Copy the project directory (so that it is on same directory level, to avoid relative issues)
2. Delete all eclipse dotted sub directories. Keep only .project and .cproject dot files.
2 Edit the .project file and change only the project name there.
Done. Now import the new project into Eclipse and do REFRESH.
2024-08-13 11:19 AM - edited 2024-08-13 11:20 AM
This is very fast and straighforward:
1. Copy the project directory (so that it is on same directory level, to avoid relative issues)
2. Delete all eclipse dotted sub directories. Keep only .project and .cproject dot files.
2 Edit the .project file and change only the project name there.
Done. Now import the new project into Eclipse and do REFRESH.
2024-08-14 8:51 AM
Thank you Pavel!
That was indeed pretty easy :)
In <proj-name>/STM32CubeIDE subdirectory I only had .osx.project (empty) and .settings/ (some prefs and language settings) in addition to .cproject and .project. I didn't bother deleting those.
File->Import->General->Existing Projects into Workspace seems to have done the trick.
2025-06-21 3:41 PM
This method looked like it was going to work until I made my changes and tried to compile. I used ADC_MultiChannelSingleConversion as the example project and created My_ADC_MultiChannelSingleConversion following the steps described. I then wanted to add LPTIM1, but could not open the IOC file until I renamed it to match my project. After adding LPTIM1, I tried to build and got
make: *** No rule to make target 'C:/ST/Another_ADC_MultiChannelSingleConversion/Drivers/STM32G0xx_HAL_Driver/Src/stm32g0xx_hal_tim.c', needed by 'Drivers/STM32G0xx_HAL_Driver/stm32g0xx_hal_tim.o'. Stop.
make: *** Waiting for unfinished jobs....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.