STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Where do I configure the GDB server log level

I have found that on one Cube installation is it 31 and on another it mysteriously changed to 1.https://peter-ftp.co.uk/screenshots/20210421153074214.jpgThe change may have been triggered by me changing between STLINK V2 and STLINK V3 and trying diff...

PHolt.1 by Senior III
  • 5841 Views
  • 6 replies
  • 0 kudos

Installing STM32CubeIDE in an enterprise environment

Has anyone deployed STM32CubeIDE in an enterprise environment, particularly to lab PCs where multiple students log into? Just wonder how you manage the workspace area and the installation of the various drivers/packages.We run Windows 10 64bit with r...

KWatt.1 by Associate
  • 1293 Views
  • 1 replies
  • 0 kudos

How to setup a STM32CubeIDE project, using X-Cube-Cellular v5.2.0, to build and including the LWIP middleware variant? (SOLVED)

I need to start from DISCOL496_RD_Sequans (or BG96) project and to wstich to LWIP stack's socket by including the LWIP middleware.As setting IDE Preprocessor USE_SOCKETS_TYPE=USE_SOCKETS_LWIP is not sufficient to include LWIP, as Eclipse generated ma...

PGell.1 by Associate II
  • 2924 Views
  • 5 replies
  • 1 kudos

After successfully added a second project to the workspace as static st32 library, I would like to know ho consume this library from the main project. From Path and Symbols I added the library ${workspace_loc:/ModuleA/Debug/libModuleA.a}.

What else should I do to let my project see header files? Is it correct to add an include path suchC:\Progetti\STM_Projects\ModuleA\Base. But I would like that it sees all the files and possible without an absolute path? What is the correct syntax?Be...

FMarr.2 by Associate III
  • 1108 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.