2021-04-29 10:26 PM
What else should I do to let my project see header files? Is it correct to add an include path such
C:\Progetti\STM_Projects\ModuleA\Base. But I would like that it sees all the files and possible without an absolute path? What is the correct syntax?
Best Regards
2021-04-30 2:01 PM
Proper way to add an archve (.a file) is the following according to me (please note ':' char is added prior library file)
Then if you want to prevent some compiler warning rely on include path to point to related .h repository
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.