2021-05-03 9:21 AM
2021-05-03 9:44 AM
Hi @BJohn.6 it may be because you don't the write access on that drive.
Try right click on the go to properties and general tab untick the Read-only attribute and click apply and ok.
May, be this resolve your issue. Or you can provide more detail about your issue by taking the snapshot of error.
Saurabh
2021-05-03 10:29 AM
This is my personal computer, not an employers. There are no read-only drives. I have tried two different drives, including the D: drive where I am doing the project development (not in the workspace). I have no problem with the actual development, It is just when I close Cube, it complains about not being able to update the workspace, (but not if it is in the C drive mess). I basically want nothing on the C drive, because I don't want to churn the SSD. The Cube complaint is apparently bogus, because I can update the tree manually. In fact, I copied it from the C: drive before I switched to it.
2021-05-03 11:57 AM
Try to create a new workspace on D: and import the project into that.
Not sure if moving the .metadata to a different drive is warranted to work.
Of course, ensure that there are no spaces or funny characters in the path.
2021-05-03 12:10 PM
I had done that previously. Nothing makes anything work. I think there is an implicit assumption that anything other than the C drive is a network drive, and it does something that does not work on a local drive. I have a hard time believing that the corporate world does not routinely put workspaces on the network for the usual reason.
2021-05-03 12:16 PM
Does the project have any "absolute paths" to includes, etc?
Change these to relative paths before moving project.
If uncertain, create a new project in new location, and look at its "includes" paths, etc.
(Backup/Zip the working project before doing anything else)
Paul
2021-05-03 1:15 PM
No. It is a simple test build anyway, and as I said before, the builld directory is not inside the repository anyway. I never do that. There is no problem with doing a build, the only problem is just Cube trying to update something in the repository. Personally, I despise the workspace concept, because it seriously complicates archival purposes to have a project split between two areas.
2021-05-03 1:25 PM
I had once also such a problem. The reason was not read only of the drive but the read only flag of a directory above was set to readonly somehow.
2021-05-03 1:47 PM
Especially in the case of the D: drive, I would long ago have noticed that issue. That is where I do most things, including email. Anyway, each case, I tried to put the workapce tree at the drive root level (except the one in C:users..., of course.
2021-05-04 4:10 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.