STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Is it possible to use TM4C123GH6PM, which is the MCU of Texas Instruments company, with STM32CubeIDE as we use in Atollic TrueSTUDIO?

Hi all,Due to GDB and OpenOCD features of Atollic, we previously imported our Keil MDK projects into Atollic TrueStudio for ARM 7.0.1. It works properly.Because TrueStudio is not recommended for new products and it is now replaced by STM32CubeIDE, we...

TERKI.1 by Associate
  • 3218 Views
  • 5 replies
  • 0 kudos

STM32CubeIDE v1.8 debug questions

I make a project with two LINKED .c source files. When debug session is started I cannot set any breakpoints inside those files. If I keep it as non linked - all OK while debugging. But this files must be linked, because it shared between two project...

ivainc by Associate III
  • 1491 Views
  • 3 replies
  • 0 kudos

Resolved! #include <numeric> fails on 9-2020-q2-update [SOLVED]

There's a bug in <numeric> library in 9-2020-q2-update toolchain. It makes the project fail to compile just by adding `#include <numeric>` to it. I also tried making a fresh new empty project with only that library included and it also doesn't compil...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.