STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE Pin Configuration/HAL Issues

I am working with the STM32F769NI evaluation kit. As expected, it comes with many more peripherals that one may need for a specific project. I have two projects which I am trying to combine together into one, both of which have separate pin configura...

repairman by Associate II
  • 4065 Views
  • 5 replies
  • 0 kudos

Resolved! Does CubeIDE supports HAL+ LL examples?

Does CubeIDE supports HAL+ LL examples? Or it is support only CubeMX? If CubeIDE it is support so, how to activate this or it is activated automatically?

DK.7 by Senior
  • 1143 Views
  • 1 replies
  • 0 kudos

Resolved! Wrong result when printing a int64_t value using STM32CubeIDE

I trying to use sprintf to display some values for debug purposes. I am getting wrong results in STM32CubeIDE v1.5.0 but it is working with an online gcc compiler.The code is in a function and for now I'm re-assigning the values inside the function f...

BTrem.1 by Senior II
  • 8874 Views
  • 3 replies
  • 2 kudos

Problem with optimal code size

Hello, I use STM32IDE to programmer for STM32F030K6, when i call the function in the main function or interrupt function, it consumes a lot of Flash.I have already changed the optimization option. But it doesn't work.I try again with Keil C and this ...

0693W00000HoFjnQAF.png 0693W00000HoFjxQAF.png 0693W00000HoFkCQAV.png 0693W00000HoFkMQAV.png
NPham.2 by Associate II
  • 7225 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.