STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Problem with creating GIT repository under STMCube IDE

I am using STMCube IDE and I fetched STM example project Lw_TCP_Echo_Server to be loaded into my STM Evaluation board Nucleo-H7S3L8. With some effort, I got it working. I want to use this project as a code base for my actual Ethernet project.I want t...

JimEno by Associate III
  • 2303 Views
  • 11 replies
  • 2 kudos

IOC tab not rendering in Ubuntu

I have a freshly installed stm32cubeide 1.13.2 on my ubuntu 22.04 machine and I've created a new workspace with a new project. In the beginning, everything works fine. But after generating code, closing the ioc file tab, closing the IDE and reopening...

Resolved! microros librart not include properly

Hi everyone,I'll start by saying I'm just starting to use STM32cubeIDE. I'm having trouble configuring the microros configuration  in my project involving an STM32F767zi board.Specifically, I managed to include everything I needed, and now when I com...

USER_RG by Associate II
  • 967 Views
  • 5 replies
  • 2 kudos

MX vs IDE possible conflicts using HAL

When using MX to generate the ioc-file and then importing it to CubeIDE, it is tricky to make it work.Such as trying to make a pin an output pin. In this case on the STM32H563 where I want to use PE2 (on pin 1) and PE3 (on pin2) as output pins. when ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.