STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

SSD1306 on SPI

Hi all,Trying to setup SPI for ssd1306 in STM32CubeIDE based on the code from "afiskon" in Github.Problem is that I'm new to this processor and the IDE.Could someone please help me?I'm using the NUCLEO-F302R8 board and I have set up the following GPI...

0693W00000WLCfpQAH.png
JSven.2 by Associate II
  • 5041 Views
  • 3 replies
  • 0 kudos

Resolved! Latest Cube IDE (V1.11.0) is taking a different .elf file and showing wrong memory regions in build analyzer. I have renamed a project long ago and have been using the new named project without any problems. Recent update is now showing older elf file

and build analyzer is showing those memory regions. I did not have this problem before. The new project name is AC_2 which is changed from AC_1. Now under build analyzer I see AC_1.elf/AC_2/Debug -27th August -2022, 6:33:40 PM. When I expand the proj...

static sack usage using command line

Hello,I know that the static stack usage is available in the stm32cubeide, but I'm wondering can I do it use a command line?after more googling, I found that there is command for arm "armlink " that can run to get the stack used for each obj file ARM...

MFawzy by Associate III
  • 2908 Views
  • 5 replies
  • 0 kudos

Resolved! to see my data on python

to see my data on python what library or code should I use in STM32(CubeIDE) ? Could you share with me example!

MFara.4 by Associate III
  • 4870 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.