STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIde freezes if a lot of data is SWV traced

HiI trace (or I try) uint32 variable (counter increased by the HOST USB interrupt) to trace MSC class problems (BTW many bugs in HAL USB Host library). I receive about 2 million traces in about 80 seconds. The problem is that eclipse if freezing and ...

0693W00000Y6kI4QAJ.jpg
pj_stm by Associate III
  • 2092 Views
  • 3 replies
  • 0 kudos

Resolved! How to debug mbed cpp program and make values visible

Hello. I am currently debugging an mbed cpp program in cubeIDE and trying to visualize the contents of variables. I was able to import from mbed to cubeIDE on my own. When I place a breakpoint on the variable I want to know about, I get the result [N...

0693W00000Y6tYgQAJ.png
hsanr.1 by Associate II
  • 2077 Views
  • 2 replies
  • 0 kudos

Resolved! [USB Host] Keyboard Output Report - How to control the 3 LEDs? (NumLock, Caps Lock and Scroll Lock status)

Could anyone tell how to add this functionality in the USB Host library for STM32CubeIDE?I found this:u8 c=3;   USBH_StatusTypeDef res = USBH_BUSY;   do { res=USBH_Set_Report(&USB_OTG_Host_Hnd,&USB_Host,0x02,0x00,0x01,&c); } while(res != USBH_OK);Sou...

by Not applicable
  • 9834 Views
  • 12 replies
  • 0 kudos

Nucleo F746 - LwIP / TCP Server

I have managed to get LwIP working and my Nucleo can be pinged and discovered via IP scanner tool. I want to get TCP/IP server working and I saw there are some files called TCP inside LwIP Library I just can get my head around it. But I have used TCP...

KPovs.1 by Associate II
  • 3014 Views
  • 1 replies
  • 0 kudos

How to generate ELF file with relative paths

Hi,I have run into a problem I can't find a solution for. Basically, I want to have in the ELF file which is generated during the build process the relative paths to the source files. Currently absolute paths are put into it to the source files, so I...

AHes.1 by Associate
  • 2479 Views
  • 1 replies
  • 1 kudos

Resolved! STM32CubeIDE: HAL lib auto update?

Hello,maybe this might be of interest to many people using CubeIDE and HAL libraries.I've seen many threads here complaining that after a CubeIDE update HAL-related sources didn't work anymore.That didn't happen to me, mostly because I don't use many...

LCE by Principal II
  • 2689 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.