STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Converting Project from Eclipse to STM32CubeIDE

I found a slightly old project, and I would like to compile it with STM32CubeIDE.It is to add HUB function in USB Host:https://github.com/mori-br/STM32F4HUBDoes anyone know how to adapt this project to compile in STM32CubeIDE?Or how to compile the or...

openocd with cmsis-dap adapter

I am in a point before on having my CMSIS-DAP openocd adapter working on CUBE IDE. But, I do not understand what I should add in order to have the CUBE's Debugger working.It seems that I need to RESET & HALT my Target in order to put it under Debugge...

JSILV.2 by Senior
  • 3213 Views
  • 1 replies
  • 0 kudos

Resolved! add arm library

hello everyoneI am a new researcher in the field and I need to develop a project with arm libraries to have some fft résultas I can find the library but i dont know how to make the project run, is there anyone who can help me?

JJuli.1 by Associate II
  • 2383 Views
  • 4 replies
  • 0 kudos

Resolved! How to export/duplicate my project from F030R8 to G070RB

hey,I Have a big Project on stm32 F030R8, and i would like to export/duplicateto a new board I have(G070RB).I am using Stm32CubeIDE, is there any magic option that it can do it by its self?Or I have to copy and past by hand (please no!).thanks in adv...

YShko.1 by Associate II
  • 1515 Views
  • 2 replies
  • 0 kudos

Can I use a USB C Breakout Board with a Nucleo board?

I'm working on a design for a custom keyboard, but I want to test as many components individually as I can before I start ordering parts. I have a Nucleo-G0B1RE (STM32G0B1), and I've carefully traced the PA11 [PA9] and PA12 [PA10] pins, and connected...

Comparing Nucleo-H743ZI2 and Nucleo-H745ZI-Q

I've written some code in STM32CubeIDE for the Nucleo-H743 which is simply toggling the board's LEDs and using the SPI channels to tx/rx with a few A/D converters. I've measured the loop's time to execute with a scope to be ~20us. I also have a Nucl...

CMcSh.1 by Associate II
  • 3935 Views
  • 6 replies
  • 0 kudos

Question on STM32CubeIDE and remote debugging

Hello, I am looking for some guidelines on how to make remote debugging possible with STM32CubeIDE running on Win10x64 and my STM32F070RB board connected to a Linux host.Everything works fine when the device is connected locally, but there is an opti...

elagano by Associate
  • 4617 Views
  • 5 replies
  • 2 kudos

Resolved! token pasting errors

I am trying to do token pasting to defined macros but it fails using this platform. main.h contains the definitions and the other file is my tokenpasting attempt getting errors but it works on netbeans

VNdir.1 by Associate II
  • 3586 Views
  • 2 replies
  • 0 kudos

How to see core utilization in stm32 cubeide?

I am using STM32L452RC for my project. I need to know the core utilization that is similar to how we see in the task manager. I need to know this, since I want to see the difference in the utilization with and without involving DMA. I need to verify ...

RAnan.3 by Associate III
  • 3446 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.