STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE Linker Query

Hi, I am planning to use the STM32L433VC processor in low power. I am planning to use SRAM2 for some data as this is preserved in low power mode. I have installed the latest STM32 CubeIDE on my laptop, and looking at the linker file it has the below ...

When I inported the project created in different PC and worked there, the error "program nullgcc not found in PATH" occurs on my PC and cannot build it. How can I fix this problem?

I also saw the similar problem "arm-none-eabi-gcc not found in PATH". I fixed this by changing the plugin path, but for nullgcc I'm not sure which path needs to be changed. I already changed some suspicious pathes. I may not have the program.

nWata.1 by Associate
  • 3366 Views
  • 2 replies
  • 0 kudos

Configure a CMake Project for the H757I-Eval

Hi, I am trying Visual Studios' new feature of importing an STM32CubeIDE Project (making it a CMake Project) and have a problem:Visual Studio Import Feature only works with single-core boards, and unfortunately, I only have dual-core boards;Anyways.....

0693W00000aIa7NQAS.png
nnoK by Associate
  • 1272 Views
  • 0 replies
  • 0 kudos

STLINK GDB SERVER Fail LiveExpression

Dear Sirs, I've just upgraded the STM32CubeIde from 11.3 to 12.0. I found an issue on my projects related to LiveExpression. I've an 32bit unsigned integer variable, but the live expression display the wrong value.I.E. if the value of the variable i...

FBign.1 by Associate
  • 1364 Views
  • 1 replies
  • 0 kudos

Resolved! Does anyone know how to update to GCC 11?

The CubeIDE 1.12.0 release notes post mentions this:"GCC update enabled – Updates GCC 11, which is already available on the Eclipse® p2 update site"I have just updated CubeIDE to 1.12.0, but GCC stays on version 10.When I click "Check for Updates" it...

cmsis_os.h and FreeRTOS.h no such file or directory

i was watching this tutorial:https://www.youtube.com/watch?v=OPrcpbKNSjUDifferences between video and what I do:my card is stm32f411re nucleo64 and i select the tim10 because the tim6 was not visible to methese are pictures: 

0693W00000BZaJcQAL.png 0693W00000BZaJXQA1.png
IDemi.1 by Associate II
  • 11044 Views
  • 11 replies
  • 0 kudos

Resolved! STM32U575 + FreeRTOS - waking up from Stop Mode

Using an STM32U575 on our own design. Aim is to put it into Stop2 Mode and wake up from three sources: a) GPIO pinb) Wake up timer (RTC)c) AlarmA (RTC) I have these three sources setup as interrupts and when the CPU is running (i.e. not stopped) thes...

JAsh.2 by Associate II
  • 7677 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.