2023-02-20 6:14 AM
Hi,
I am planning to use the STM32L433VC processor in low power. I am planning to use SRAM2 for some data as this is preserved in low power mode. I have installed the latest STM32 CubeIDE on my laptop, and looking at the linker file it has the below when cerating a new project. As the RAM of the processor is 64k , and the data sheet mentions the RAM2 16k is part of the 64 k. But looking at the below it says the RAM is 96K.
Latest STM32 CubeIDE:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 256K
}
And pointed my data to SRAM2 as below.
typedef struct{
long date;
long time;
short int hum;
short int temp;
}Results;
char Buff[sizeof(Resukt2)*500] __attribute__((section(".readings_buffer")));
SECTIONS
{
.readings_buffer :
{
KEEP(*(.readings_buffer))
} >RAM2
My atollic STM32 CubeIDE I have been using in years just created the new project for the same processor:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 256K
}
Which indicates 64k ram, can someone please explain what is happening to the 96k above
Shouldnt the link file be:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 48K <<< as RAM2 is part of the 64k
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 256K
}
Best Regards
Scott
2023-03-09 5:33 PM
STM32L433 has 64kB SRAM composed of SRAM1 (48KB) and SRAM2 (16kB).
As described in datasheet section 3.5:
• 48 Kbyte mapped at address 0x2000 0000 (SRAM1)
• 16 Kbyte located at address 0x1000 0000 with hardware parity check (SRAM2).
This memory is also mapped at address 0x2000 C000, offering a contiguous address space with the SRAM1 (16 Kbyte aliased by bit band)
This block is accessed through the ICode/DCode buses for maximum performance.
These 16 Kbyte SRAM can also be retained in Standby mode.
So you have 2 ways to configure the linker file for RAM space:
Option #1: RAM2 is used for code execution
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 48K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 256K
}Option #2: RAM2 is used for data storage and application take benefit of the full RAM
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 256K
}As your intent is to use SRAM2 for data storage, then I suggest you use option #2.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.