STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! std::string causing compilation errors

Hi, I'm writing a simple uart controlled oscillator.However when Including std::string, basic_string.h and stl_iterator.h causes several errors.it almost looks like something is not included, like remove_const_t add_const_t etc..In these errors, GLIB...

I am using Nucleo STM32F767ZI board. I am making a custom HID application. I am able to send data to game controller, if I use while(1) loop in the main function. But unable to send data using interrupt/polling method. tried to write and send buffer in Ou

I am using Nucleo STM32F767ZI board. I am making a custom HID application. I am able to send data to game controller, if I use while(1) loop in the main function. But unable to send data using interrupt/polling method. tried to write and send buffer ...

ATamb.2 by Associate II
  • 1415 Views
  • 2 replies
  • 0 kudos

Resolved! L432KC - Encoder not counting?

I am trying to use a Nucleo L432KC board's hardware timers with a rotary encoder. Specifically I am trying to use TIM1, pins PA8 (D9) and PA9 (D1). I was originally hoping to use PlatformIO and the gianni-carbone/STM32encoder library, but when I coul...

HMorg.1 by Associate II
  • 2658 Views
  • 2 replies
  • 0 kudos

Execution error when I declare many extern variable.

I'm working with a STM32F407 and CubeIDE. My program is divided in various small .c files. This cause a lot of extern variables declarations. Recently the programm presents erronious behavior when I create a new extern variable declaration, but with ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.