2023-03-12 11:12 PM
Hi, I'm writing a simple uart controlled oscillator.
However when Including std::string, basic_string.h and stl_iterator.h causes several errors.
it almost looks like something is not included, like remove_const_t add_const_t etc..
In these errors, GLIBC THROW is used against c++17 spec, it's strange since the project was generated by the STM32CubeIDE, and I'd assume the accompanying library would be compatible with the c++ standard set as default by the same ide.
Errors In question:
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\bits\stl_iterator.h:2307:26: error: 'remove_const_t' does not name a type
2307 | using __iter_key_t = remove_const_t<
| ^~~~~~~~~~~~~~
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\bits\stl_iterator.h:2319:10: error: 'add_const_t' was not declared in this scope
2319 | pair<add_const_t<__iter_key_t<_InputIterator>>,
| ^~~~~~~~~~~
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\bits\stl_iterator.h:2319:22: error: '__iter_key_t' was not declared in this scope; did you mean '__iter_val_t'?
2319 | pair<add_const_t<__iter_key_t<_InputIterator>>,
| ^~~~~~~~~~~~
| __iter_val_t
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\bits\stl_iterator.h:2319:35: error: wrong number of template arguments (1, should be 2)
--ommitted--
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\bits\basic_string.h:531:27: error: '_RequireAllocator' does not name a type
531 | template<typename = _RequireAllocator<_Alloc>>
| ^~~~~~~~~~~~~~~~~
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\bits\basic_string.h:531:44: error: expected '>' before '<' token
531 | template<typename = _RequireAllocator<_Alloc>>
| ^
--ommitted--
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\new:126:52: error: ISO C++17 does not allow dynamic exception specifications
126 | _GLIBCXX_NODISCARD void* operator new(std::size_t) _GLIBCXX_THROW (std::bad_alloc)
| ^~~~~~~~~~~~~~
c:\st\stm32cubeide_1.12.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\new:128:54: error: ISO C++17 does not allow dynamic exception specifications
128 | _GLIBCXX_NODISCARD void* operator new[](std::size_t) _GLIBCXX_THROW (std::bad_alloc)
| File that uses std string:
#ifndef __H_FILE
#define __H_FILE
#ifdef __cplusplus
#define EXPORT_C extern "C"
#else
#define EXPORT_C
#endif
EXPORT_C void _main();
EXPORT_C void _onUsart();
#ifdef __cplusplus
#include "stm32l4xx_hal.h"
#include "stm32l4xx_ll_usart.h"
#include "stm32l4xx_ll_gpio.h"
#include "main.h"
#include <string>
class main_c
{
private:
main_c()
{}
public:
static inline main_c& getInstance()
{
static main_c instance;
return instance;
}
void main(void)
{
LL_USART_EnableIT_RXNE(USART2);
LL_USART_EnableIT_TXE(USART2);
__enable_irq();
LD3_GPIO_Port->ODR = LD3_GPIO_Port->ODR ^ LD3_Pin;
}
void onUsart(void)
{
if (USART2->ISR & USART_ISR_RXNE)
{
recieveBuffer += USART2->RDR;
}
if (USART2->ISR & USART_ISR_TXE)
{
if (transmittPointer < transmittBuffer.size())
{
USART2->TDR = transmittBuffer[transmittPointer++];
}
}
}
void print(std::string text)
{
while (transmittPointer < transmittBuffer.size())
{}
USART2->TDR = transmittBuffer[transmittPointer++];
}
std::string recieveBuffer;
std::string transmittBuffer;
size_t transmittPointer = 0;
};
#endif
#endif
Solved! Go to Solution.
2023-03-12 11:17 PM
Ah I've figured it out, an added library redefined __cplusplus define, which contains the version of currently used C++.
so glibcxx was configured to the wrong c++ version :p
2023-03-12 11:17 PM
Ah I've figured it out, an added library redefined __cplusplus define, which contains the version of currently used C++.
so glibcxx was configured to the wrong c++ version :p
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.