STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Not all power regulator voltage sources available for STM32H755

Hi,In the device configuration tool for the STM32H755 I'm not getting all the power voltage source options, severely limiting the clock speed of the CPU. For some reason the options that are there are grayed out, and I'm missing 1 and 0. My clock con...

tomseli_1-1689154876828.png tomseli_2-1689154902018.png
tomseli by Associate
  • 3131 Views
  • 5 replies
  • 0 kudos

Stm32F7 USB HOST USB DISK f_mount cause HardFault_Handler

HiI have a custom board with STM32F799 and USB host device for read a data file from flash Key.The development software is STM32CUBEIDE V1.13.0The firmware include TouchGFX with FREETOS V1 for manage a graphix display.I configured USB_Host for Mass s...

PZamb.2 by Associate III
  • 1348 Views
  • 0 replies
  • 0 kudos

Resolved! How to set up FreeRTOS debugging using STM32CubeIDE

Hi, I'm trying to debug a FreeRTOS program and coming from a Keil + STM32CubeMX world, I'm having trouble setting up any of the eclipse based IDES to use the FreeRTOS thread aware debugging tools. So far, I've tried a combination of using the StateV...

Resolved! Live expression write value

I'm pretty sure that this is not implemented yet, but it would be extremely helpful to do so. I want to write the variables through the live expressions tab in the debugging mode, like I'm used to do in the IAR EW.If this option is already available ...

TKleg.2 by Associate II
  • 2393 Views
  • 2 replies
  • 0 kudos

About unknown errors

Hi ,What does this error represent?Also, what should I do to eliminate this error? I am currently trying to control the motor of FOC in Cube IDE and workbench.The cause of this error is unknown, and even if you proceed according to the video on the w...

Nishino08 by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos

System supply configuration: set LDO Supply in STM32CubeIDE

Hello,I have designed my own board with a STM32H7 MCU and set the "System supply configuration" to "1. LDO Supply selected" (see picture).In the STM32CubeIDE in the IOC file under the item System Core - RCC the SupplySource is set to PWR_LDO_SUPPLY. ...

Pic1.PNG
TBend.3 by Associate II
  • 5105 Views
  • 5 replies
  • 0 kudos

Resolved! USB CDC example for STEVAL-WINBOX1 (STM32U585AI)

Hi all,I'm new in programming STM32U585AI.Bought the STEVAL-WINBOX1 and as first step tried to have working USB CDC.Since didn't find code example in STM32CubeIDE for this specific dev kit, create a new new project based on example Ux_Device_CDC_ACM ...

Adeuga by Associate II
  • 4462 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.