STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't paste text into Cube IDE main.c file

I need to copy text from internet to Cube IDE main.c file.I copied the text from the internet, I click in the Cube IDE context menu "paste". And nothing happens. If I copy text from Cube IDE and paste that text into Cube IDE, then the text is pasted....

tim2.png
MMust.5 by Senior II
  • 3321 Views
  • 5 replies
  • 1 kudos

Resolved! Invalid Input: Must be project's active .ioc file.

Hi,i want to clone my project. I did the following steps:1) Edit > Copy.2) Edit > Paste.3) Rename the ioc files.4) Delete the Debug.launch file.5) Project > Clean.the next step is to generate the CubeMX. But when I try to open the .ioc file this erro...

MStre.1 by Associate II
  • 21235 Views
  • 11 replies
  • 4 kudos

Debogage

 Hello,I've developed a program using the I-CUBE LRWAN package, but I'm having a problem debugging it. Here is the configuration I used for debugging:The errors I'm encountering are as follows:STMicroelectronics ST-LINK GDB server. Version 7.3.0Copyr...

2.png 1.png
eljohrikm by Associate II
  • 2712 Views
  • 5 replies
  • 0 kudos

Unable to get RTC interrupt with STM32L476.

Hello!I am trying to get interrupt on each second using STM32L476 RTC module.I am configuring RTC module using cubeMX.RTC module interrupt is enabled, but there aren't any interrupts from RTC?!Would you please advice!

LMehm by Associate III
  • 4321 Views
  • 3 replies
  • 0 kudos

Resolved! Changing from 144-in processor to 100-pin processor

I have a project that uses a STM32H743ZITX (144-pins). I want to replace it with a STM32H743VITX (100-pins), and use the same same code. There will actually be a few differences in code, like removing some pins and their functions, but it's pretty mu...

hwsw by Associate II
  • 1898 Views
  • 1 replies
  • 0 kudos

Error in GPIO functions

 It seems the IDE is not able to use the ADC and any functions related to it - my error is that the ADC libraries are not importing properly We are using the HAL libraries.. Additionally, the GPIO and any functions related to it are not being support...

acai by Associate II
  • 5618 Views
  • 7 replies
  • 1 kudos

Multiple linker symbol error after update to CubeMX 6.9.0

After Upgrading to Cube 1.13.0 with CubeMX6.9.0, my project is no longer compatible with CubeMX 6.8.1.When I start the CodeGenerator, it creates a file \Drivers\CMSIS\Device\ST\STM32H7xx\Source\Templates\system_stm32h7xx.cwhich is a duplicate for the...

JojoS by Associate III
  • 1431 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.