STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Loading problem with STM32CubIDE_1.14.0

Hi,I'm trying to get running with a STM32F446. I'm using a Nucleo 64 board for now. I've installed CubeIDE on a new computer running Windows 10 and I get Make error 2 and the messages that it can't find gcc and g++. It seems to be a problem with path...

Resolved! Run/Debug don't work

Hi,I've STM32CubeIDE v1.14.1 on a Windows10 PC. I've NUCLEO-G0B1RE board and I've created my workspace with a standard project starting from the NUCELO ioc configuration. I can build the project and upload the .elf file on the uC with STM32CubeProgra...

problem.png
BRonc.1 by Associate III
  • 9083 Views
  • 18 replies
  • 1 kudos

Resolved! NUCLEO-G0B1RE and USB HID function

Hi,I would like to enable the USB HID Device function to the target uC of the NUCLEO board. So I've created a new project, selected the board and added the 2 USB pin configuration:I've also enabled the middleware functions:the clock config seems to b...

BRonc1_0-1705677489698.png BRonc1_1-1705677509499.png BRonc1_2-1705677570198.png BRonc1_3-1705677632449.png
BRonc.1 by Associate III
  • 2019 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIde Failed to start GDB Server on STM32F103C8

hello,I have the same problem posted by H.Ahmed on October 2022, read also in other posts:"Failed to start GDB Server Error Initializing ST-LINK deviceReason (18) Could not verify ST device!"I tried all suggestions found on web, but no help.I'm using...

Mauri by Associate II
  • 20845 Views
  • 12 replies
  • 0 kudos

Major Bug when erasing a projet

how to reproduce:Create a new projet with a "namePrj" and "directory". The normal way should be to have a directory "directory"/"namePrj", and in this directory, all the project files (like with STM32CubeMX). But the files a created in the "directory...

ANauz.1 by Senior II
  • 5139 Views
  • 11 replies
  • 2 kudos

ST-Link upgrade error on Nucleo F446RE

I run CubeIDE on Linux and when I want to Debug, it prompts for an ST-link upgrade. I click Yes and I get screenshot no. 1. The ST-LINK ID displayed there is correct, I get the same ID with "st-info --probe".Then I click on Open in update mode, and I...

aro by Associate III
  • 7243 Views
  • 9 replies
  • 0 kudos

Why is STMcubeIDE not detecting my device?

Hi all, I am trying to run a program from STM32cubeIDE to my STEVAL-MKI109V3 board, however the IDE is not recognizing my board. The device is listed in Device Manager under Ports&COMs as "STMicroelectronics Virtual COM Port (COM5)" so this leads me ...

ZoeTakacs by Associate II
  • 1608 Views
  • 1 replies
  • 1 kudos

stm32cube to compile legacy arm syntax?

Hi folks,I have an assembly file with 2.5k lines and I'm facing a compiling issue.It seems that the problem is about the syntax -GNU compilation support a specific syntax while arm leagacy syntax is different. In example:name EQU 0xC vs.equ name 0xC ...

kingkong by Associate
  • 1943 Views
  • 2 replies
  • 0 kudos

[STM32WL55] Boot in low power mode.

Hello everyone!I'm wondering about a possible solution for our device working on a STM32WL55.For hardware reasons, it would be nice to boot the device directly in low power mode (possibly STOP2).I can't seem to find any answer to this question online...

LorenzoC by Associate
  • 968 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.