2024-01-17 9:17 AM
hello,
I have the same problem posted by H.Ahmed on October 2022, read also in other posts:
"Failed to start GDB Server Error Initializing ST-LINK device
Reason (18) Could not verify ST device!"
I tried all suggestions found on web, but no help.
I'm using STM32CubeIde 1.14.1, ST-Link V2 (updated)
Connection is very simple and should be OK, because if i program the device wth ST-Link Utility
or with STM32CubeProgrammer, all works fine.
I tried with CubeIde 1.8.0 as suggested in another post, but no luck.
Even older projects who i made some years ago, now have the same problem.
I read also on a post that someone from ST apologizes for this problem who is an older
bug reappeared now.
Hope there is a solution, because it would be very frustrating if i'm constrained
to change an IDE who i love, and if i'm unable to mantain older projects.
Thanks in advance
elvisee
Solved! Go to Solution.
2024-01-18 2:58 PM - edited 2024-01-18 2:59 PM
Hello @Mauri
To have the most probable device marking for each product. Check the product Package then refer to the TN1433 for verification.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-17 10:06 AM
If you have a counterfeit programmer, that's probably the issue. Falling back to a ~2 year old STM32CubeIDE version would fix. Buying a legit programmer would also fix.
2024-01-17 10:06 AM
Hello @Mauri
Are you sure that you are using a genuine product. Such a problem can happend if you are using a clone one as mentionned here.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-18 1:26 AM
Yes, it's a genuine ST-LiNK V2. I have 2 of them and both work well with CubeProgrammer and ST-Link Utility, but not with IDE
2024-01-18 1:34 AM
2024-01-18 6:19 AM
You sure? There's no ST product named "ST-LiNK V2". Can you link to what you have or post a picture?
2024-01-18 6:48 AM - edited 2024-01-18 6:50 AM
>Is there a sign of non genuine product?
Yes, because IDE refuses to work with this (wrong cpu inside) st-link.
ST-link utilty (old...) + CubeProgrammer not checking (until now) original or not, so they still work.
+
The st-link V2 "sticks" work ok also with IDE, if there is a STM32F103 inside;
i know, because i have some of these !
But also some with a CK32F103 , here IDE tell you the story about wrong product...
So buy a new st-link V3 , or if want cheap, a st-link V2 "fake" (but verify, it has genuine stm32f103cb inside! )
2024-01-18 1:13 PM
AScha.3 Thank you for reply.
The ST-Link V2 is original.
Normally i used the sticks, but since CubeIde 13 it requires FW upgrade, and the sticks don't accept upgrade, because, yes they are CK32F103,
But since 1.13.0 i use only the original ST-LINK V2, with the most recent FW (today V2J4357).
I uninstalled and installed more times CubeIDE 1.8.0, 1.13.0, 1.14.0 and now 1.14.1.
But if after uninstall something is not totally clean? Maybe Windows10 or CubeIDE saves something (registers or so), who remenbers this problem?
What's your opinion?
thank you very much
2024-01-18 1:49 PM - edited 2024-01-18 1:49 PM
If nothing else helps, get a J-Link or ST-Link v3.
2024-01-18 2:23 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.