STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to change the Repository path in CubeIDE?

Hello community, I have a problem with new project creation, whenever I want to create a new project I come across this error: create minimal project failure: cannot read template source. reason: internal error i know the problem which is having a sp...

JBazm.1 by Associate III
  • 22262 Views
  • 12 replies
  • 6 kudos

HAL_Delay() affecting function execution times

Hi,I'm trying to measure the execution time of an algorithm using the Cortex-M7 on a Nucleo-H745ZI-Q. I'm measuring the execution time using a GPIO pin and the DWT cycle counter register. Here's the form this profiling takes in my while (1) loop.I'm ...

stn_3-1705884655731.png
stn by Associate
  • 2338 Views
  • 2 replies
  • 0 kudos

Resolved! Frustrated at the staring post

Today, I tried installing CubeIDE so I could get a sample project up and running to evaluate against a Nucleo 144 board.  This is my second attempt, and both times I get this error.  Nothing in the manual, cannot find nothing on Google either.  The I...

gerrysweeney_0-1705870789996.png

Resolved! SPI master interrupt issue

Recently working with spi communication in stm32g070rb using stm32CubeIDE (HAL library).SPI master receive interrupt triggered continuosly when there is no interrupt.But same code wrote in SPI slave its works perfectly.I also put Pull down resistorso...

vignesh1 by Associate III
  • 4566 Views
  • 5 replies
  • 1 kudos

upgrading FreeRTOS in CubeMXIDE

FreeRTOS is currently at 11.0.  The version in CubeMXIDE is 10.3.1.  There are some good features in 11.0 I'd like to use, so the following questions:11.0 is supposed to be a drop in replacement for 10.6.1  I'd do a download, unzip the files, and jus...

Gitignore in CubeIDE. What files do you like to ignore?

Which files/folders to you like to put in .gitignore ?I tend to put: Debug and Release because I'm happy to rebuild on new platforms. But, I also put Drivers and Middlewares since they can also be sourced from ST repos.I'm wondering also how people m...

DJC by Senior
  • 6158 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.