STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Signal Pass through using ADC and DAC

The equipment I am using is the following: Nucleo-Board L476RG, STM32CubeIde 1.10.1. I am attempting to design a simple dsp system that uses an ADC to send the data it receives from a function waveform generator to a DAC, and the DAC output will then...

JEscu.2 by Associate II
  • 6360 Views
  • 7 replies
  • 0 kudos

Refresh files to compile after prebuild steps

I run my python script in C/C++ Build --> Settings --> Build Steps --> Pre-build steps by running command:cd ${ProjDirPath}/menu_language_generator && python generate.pyThis script generates header files to my project with langauge translations. Scri...

DBrau.2 by Associate III
  • 1544 Views
  • 2 replies
  • 0 kudos

"Dwarf Error" error after new installation

 Hello friends, thank you for your help.My main problem is that none of the new projects I open on my newly installed STM32Cube on my computer work, but when I import my old projects, they work.part number: stm32f103c8 Environment: STM32CubeIDE / Ver...

WhatsApp Image 2025-02-26 at 11.39.14.jpeg PROG.PNG ERROR.PNG pac.PNG
Sözde.11 by Associate II
  • 1722 Views
  • 2 replies
  • 0 kudos

Unable to Download STM32CubeIDE

Hi everyone,I'm having trouble downloading STM32CubeIDE. Even though I'm registered, There seems to be somthing broken with the Web page.I’ve tried multiple browsers, but still no luck. I also haven’t received any email with a download link.I’ve been...

cerine by Associate II
  • 3084 Views
  • 6 replies
  • 1 kudos

Stm32H747I-DISCO Share Peripherals

Hi Is it possible to share some peripherals between cores?My goals is to share the SD card  trought CM7  and CM4 using hardware semaphore for the access(one SD hardware but both cores can write and read on it sharing the SD pins).Using Stm32CubeIDE i...

DMazz.1 by Associate II
  • 1162 Views
  • 2 replies
  • 1 kudos

Resolved! SDRAM and a global struct.

Hi.I am using TouchGFX and it works fine,My MCU is STM32H743 But when I use the SDRAM for other things the code does not work.My question is:Can I use struct in the  SDRAM.? I have this one in my c file.  SD_CARD SdCard __attribute__((section("\"SDCa...

Hector_R by Associate II
  • 3734 Views
  • 10 replies
  • 0 kudos

Resolved! CubeIDE issue with timers

Hello,I'm facing a very annoying issue in CubeIDE.Board: Nucleo-F412ZH.The project uses TIM1 Channel4 to genrate a Stream of PWM pulses to drive a WS2812B LED strip using DMA.It also uses TIM9 to generate the systick.With this configuration, the MCU ...

zeboss49 by Associate III
  • 2189 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.