STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer v2.16.0 released

STM32CubeProgrammer v2.16.0 release informationNew features:• Added the support for the STM32U0 series– Flash memory/option byte/OTP programming via the debug and bootloader interfaces– RDP regression with password• Added the support for the STM32H7R...

STM32MP135

I would like to Design STM32MP135FA Processor based data logging and file accessing throgh Ethernet Kinldy suggest below application possible in STM32MP135 series Processor.1. Two ethernet going to use - One for SD card file acess / another one for F...

JMari.11 by Associate
  • 1892 Views
  • 1 replies
  • 0 kudos

RNG1 probe error: Configuration incorrectly allows both A7S and A7NS to be selected simultaneously

We're using the ST v5.0 eco-system and v.6.9 of STM32CubeMX.Per RNG internal peripheral - stm32mpu, the RNG1 peripheral should be a single choice assignment. When I click on A7S (OP-TEE), the tool warns me that it cannot be removed from the A7S conte...

SLivi.1 by Associate II
  • 4034 Views
  • 4 replies
  • 2 kudos

Resolved! DDR_Init_A7 unable run

DearsI can only start this example in Debug mode, the BLUE led start blinking... So it works OK.But If I try to use RUN command (using icon, or right mouse click on project file) than it seems not work (RED leds blinks only ONE and is OFF, Blue LED i...

ravo by Senior
  • 3143 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.