2023-07-20 7:48 AM
I would like to Design STM32MP135FA Processor based data logging and file accessing throgh Ethernet
Kinldy suggest below application possible in STM32MP135 series Processor.
1. Two ethernet going to use - One for SD card file acess / another one for Firmware update / web or ofline GUI in
2. Linux based system which should be boot from eMMC or NAND flash or DDR3 ( Except SD card)
3. Linux booting should be work in within 6-10 seconds time line.
4. Power back for power shutdown option , so that any PMIC suggest.
5. Internally SQL Database going to store the logging data, so file transfer should be 10MBit /Sec thorugh Ethernet.
6. 2 CAN FD + 4 UART+ SPI+ RTC+USB+ SDRAM addtional interface and pheriperals.
7. whether Linux boot on this processor avaiable other than SD card Memory?
Please give your suggestion for start the design , also suggest any advance PMIC for avoid the Lunix booting /Runnig file correption.
Waiting for your valuable answer.
Thanks you ... by Jagathguru Marimuthu
2024-03-18 7:11 AM
We are also looking like this configuration, Could you please share information if you done
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.