2019-07-04 7:08 AM
Koan is proud to provide the unofficial Yocto Project BSP for STM32MP1 based boards.
This project is not endorsed nor supported by ST.
ST OpenSTLinux is based on OE, our BSP extends the use of ST meta layers with Yocto, using latest commits on the branch 2.6 'thud' on each meta layer.
At the moment only ST's defined distros and images are supported out-of-the box, but you can work also with Poky ones with a little more effort.
One of the most interesting features of this approach is to have the Qt5 (release 5.11.2) support on the board and being able to generate a redistributable SDK toolchain to compile your Qt5 applications.
See our recent post about it : http://www.koansoftware.com/en/content/yocto-project-meta-layer-stm32mp1-koan
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
2019-09-25 1:31 AM
Are you using this repo? Add a like!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.