2026-03-25 12:31 AM
Dear ST Community,
I am currently working on a custom hardware design based on the STM32MP157CAC3 MPU, which includes LPDDR3 memory (Micron MT52L256M32D1PF) and multiple high-speed interfaces.
As part of my signal integrity and high-speed design validation process, I need simulation models to conduct accurate analysis.
I want to request the following:
IBIS models for STM32MP157CAC3, specifically covering:
1. DDR interface (LPDDR2/LPDDR3 controller)
2. SDMMC interface
3. Any other relevant high-speed I/Os(MIPI, LTDC, DCMI, SDMMC)
S-parameter models (if available) for:
1. High-speed I/O buffers
2. DDR interface pins or PHY
Any additional resources that may support SI/PI analysis, such as:
1. IBIS-AMI models (if available)
2. Reference simulation setups
3. Application notes related to DDR signal integrity
Project details:
Custom PCB (not a direct copy of STM32MP1 DK2)
LPDDR3 operating btw 300 - 800 MHz
Goal: Pre-layout and post-layout SI validation (HyperLynx/ADS
I understand that some of these models may require NDA access. I am willing to follow the necessary process if required.
Please let me know the appropriate steps to obtain these files.
2026-03-25 1:09 AM
Hi,
What you are asking for is already available in the product page (https://www.st.com/en/microcontrollers-microprocessors/stm32mp157c.html), e.g.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.