STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question about the network.

I need a network connection for my project. Does the network PHY have to be programmed in CM4 via LwIP ... or does communication via OpenAMP to the CA7 work? Are there examples of a simple web server that can switch a port or similar? Thank you very ...

RSeit by Associate
  • 2353 Views
  • 2 replies
  • 0 kudos

Why Flashing the FSBL Failed?

I have a DK2 board.Downloading FSBL image for EV1 board to DK2 board through USB port on DFU by the STM32CubeProgrammer fails. Both boards use the STM32MP157C chip, but I don't understand why the download fails.Can anyone explain the reason or princi...

SCho.3 by Associate
  • 1525 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP Computing Module Request

I was thinking that it would really useful if there was a ready to use Raspberry-Pi computing module look alike STM32MP board which could be used in development of user applications.The reason is because although ST has designed MP series to be optim...

Resolved! proper way to read /dev/ttyrpmsg0

Hi,I am executing echo_tty_echo example and trying to get the messages coming from m4 inside qt program as follows:   QString line;   QStringList list1;   char buff[100];   while (1) {       QProcess::execute("echo hello > /dev/ttyRPMSG0");       QFi...

IYetk by Associate III
  • 1303 Views
  • 1 replies
  • 0 kudos

STM32MP1 TFT settings

I want to change resolution of display in ev kit but don't know how to do.Should I change the default struct values in panel-raydium-rm68200.c or is there another method? Also, I'd like to rotate the screen of TFT so it will be wide screen TFT, is it...

Resolved! Low power mode on 'basic' image

Hello.I've created basic image with FlashLayout_sdcard_stm32mp157c-dk2-basic.tsv from stm32mp1-openstlinux-4.19-thud-mp1-19-02-20 downloaded from site. And I can't normally enter to any low power mode: stop - "systemctl suspend" or "echo mem > /sys/...

alexey.b by Associate II
  • 1885 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.