STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Failed to run code in DDR of STM32MP135F-DK?

Running the code "MP13_BSP_BasicTemplates" in the DDR of the STM32MP135F-DK succeeds,But running the code "UART_Receive_Transmit_Console_A7" in the DDR of the STM32MP135F-DK fails(“USE_DDR” Macros added,Link text has been modified),Errors are as foll...

微信图片_20240603163959.png
zhuij.1 by Associate II
  • 1537 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP15x PWM with DMA

Hi,I am using a STM32MP151AAA3 and i need to control an RGB LED via PWM control (something like the WS2812B). I was looking into the PWM driver options for Linux side control and can't find options for PWM control for specific buffer sizes or anythin...

RBerk.1 by Associate III
  • 2144 Views
  • 2 replies
  • 0 kudos

Resolved! multiple ADC for gpio

Hi!! I have STM31mp157C and I want to use the ADC. I am exploring the available GPIOs and have observed that some are present in both ADC1 and ADC2.For example, according to the datasheet, PA4 can be used with ADC1/ADC2.Is there any difference betwee...

unnamed.png
AVazquez by Associate III
  • 2651 Views
  • 2 replies
  • 0 kudos

ES8388 codec cannot get mclk

Dear community,I need your help.I'm using a ES8388 Codec on a custom board with STM32MP157 MPU. ES8388 codec connected on i2c1 and sai2. In the codec driver, ES8388 is in salve mode and MPU is in master mode. mclk cannot be obtained.​​device tree:​k...

0693W00000QKqJiQAL.png 0693W00000QKqKHQA1.png 0693W00000QKqKWQA1.png 0693W00000QKqQ5QAL.png
ZLiu.3 by Associate II
  • 9475 Views
  • 13 replies
  • 0 kudos

STM32MP153 Can't wake up from CStandby

Hi there, I'm using a custom STM32MP153 board with OpenSTLinux distribution (5.15.24) on it, and  I have a problem with the Wake UP. I successfully set PWR gpio to wake up from low power modes. In fact, I can successfully wake from CSleep and CStop m...

SScar.2 by Senior
  • 1159 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.