cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP153 Can't wake up from CStandby

SScar.2
Senior

Hi there, 

I'm using a custom STM32MP153 board with OpenSTLinux distribution (5.15.24) on it, and  I have a problem with the Wake UP. 

I successfully set PWR gpio to wake up from low power modes. In fact, I can successfully wake from CSleep and CStop mode. But I can't execute a correct wake up from CStandy mode. (setting from M4 firmware is OK I think, I took the example code from FW1.6.0 repo) 

Is there any common pitfall that I must be awared of?  

NOTE: I'm using STPMIC1 . 

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0