STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 userspace GPIO control

Hello everyone, I was attempting to migrate my existing raspberry pi application for GPIO control to the STM32MP157 but I encountered a roadblock. I was using gpiod to drive the pins from the userspace app but the following guide:https://wiki.stmicro...

Use rotary encoder on stm32mp157

 I'm doing a project, that I need a rotary encoder working on cortex-a7 core of stm32mp157.I met problem, my rotary encoder can not work. This is what I have done:1. In kernel menuconfig I have config: use rotary encoder as a build-in module;2. Write...

Jason007_1-1716992523494.png Jason007_1-1716992931386.png Jason007_0-1716992396373.png
Jason007 by Associate
  • 1616 Views
  • 1 replies
  • 0 kudos

Resolved! CMD Line Disable on STM32MP131

I am using the SDMMC1 interface without an SD card, utilizing only the data lines. Therefore, the CMD line is not needed, and I have deactivated the CMD pin. However, the HAL_SDMMC library sends CMD data and expects a response from the SD card, causi...

Stnoobs by Associate II
  • 4714 Views
  • 3 replies
  • 0 kudos

Clean shutdown of M4 core

Hello all,The startup of the M4 core is easy enough, echoing "start" to the state enables the core.Shutdown is also simple, echoing "stop" to halt the coprocessor. However on shutdown, peripherals such as the PWM sometimes end in a high state. For my...

csys by Associate
  • 2643 Views
  • 3 replies
  • 1 kudos

Resolved! STM32MP13 Line ST-Link Possible Version?

 Hello, I am in the process of planning and testing the STM32mp13 Line.We have equipped our project board with the STM32mp13 CPU, but we encountered an issue when trying to connect it via St-link; it did not establish a connection.The St-Link version...

SL1 by Associate III
  • 3716 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.