STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am tring to rebuild kenel for STM32MP157C-DK2 PC $> make ARCH=arm multi_v7_defconfig fragment*.config

[   1.825627] usbhid: USB HID core driver[   1.833630] stm32-ddr-pmu: probed (ID=0x00140061 VER=0x00000010), DDR@533MHz[   1.840775] optee: probing for conduit method from DT.[   1.844463] optee: api uid mismatch[   1.848396] NET: Registered protocol...

建胡.1 by Associate
  • 1404 Views
  • 1 replies
  • 0 kudos

Multiple camera interfacing

Hi all,I understand that it is possible to interface a CSI2 camera sensor with the camera interface of STM32MP1 using STMIPID02 chipset. Even-though this later support 2 cameras, I'd like to know that it is feasible from the MPU's point of view ?Than...

KLe T.1 by Associate
  • 2649 Views
  • 2 replies
  • 0 kudos

Resolved! after rebuild kernel then machine stop to Waiting for here root device /dev/mmcblk0p6...

I am tring to rebuild kenel for STM32MP157C-DK2 using below url. ​https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernelAfter I did 5.4 ...

bkwak by Associate II
  • 9259 Views
  • 15 replies
  • 0 kudos

STM32 TF-A FSBL customization workflow

I need to customize the TF-A en.SOURCES-tf-a-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xzOur custom board have a different pin selection for UART4 debug as you can see below, the UART4_TX pin is not on the STM32_PINMUX('G', 11, AF6), but is on ...

koan by Associate III
  • 4908 Views
  • 8 replies
  • 0 kudos

Flash SD(TF)-card over USB adapter.

On most cases the script "create_sdcard_from_flashlayout.sh" futile. Built-in card reader today is preliminary remains on notebooks. As result very often a sd-card used over a usb adapter. On a remote virtual machines always it will be used over a c...

KSuch.2 by Associate II
  • 1940 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.