STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Examples for STM made OP-TEE drivers?

Hi all,i want to use some hardware peripherals in OP-TEE. I got the GPIO driver (stm32_gpio in core/drivers) to work with my PTA (Pseudo Trusted Application). I now wanna use the I2C peripheral using the stm32_i2c driver.I coundn't find any example c...

Fee by Senior
  • 2737 Views
  • 4 replies
  • 0 kudos

UART4 RX Signal level

I use the UART4 like the following initialization.​void uart4_configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; /* enable usart clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENAB...

0690X00000DYODdQAP.jpg 0690X00000DYODiQAP.jpg
Kim.Andy by Associate III
  • 4381 Views
  • 2 replies
  • 0 kudos

Resolved! bitbake error

I'm referring to the following website.https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_PackageI stumbled on "6 Building the OpenSTLinux distribution".Error occurred in bitbake.I attach the log.Could you tell me the cause of the error?Bes...

Osamu by Associate II
  • 2214 Views
  • 2 replies
  • 0 kudos

Control external amplifier via GPIO

HI all,I am using an STM32MP15-EV1 eval board and will connect an external amplifier to the HEADSET output. I would like this amplifier to be automatically switched on / off when sound is being played. If I am correct this is supported in the audio-g...

Resolved! Linux Kernel build failure.

I’m getting a build error when attempting to build the linux kernel.ERROR:scripts/extract-cert.c:21:10: fatal error: openssl/bio.h: No such file or directory #include <openssl/bio.h>I have followed instructions from https://wiki.st.com/stm32mpu/wiki/...

JSpra by Associate III
  • 7711 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.