STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debug on STM32MP1 issue

Hi,We are currently developing on the STM32MP1. Our goal now is to be able to debug the core at the different running stages : TF-A, Optee, U-boot and kernel. We are using the DK2 with a ST-link and openOCD.When using your Setup.gdb we experience som...

romain2 by Associate III
  • 3200 Views
  • 2 replies
  • 1 kudos

Best way to Flash the M4 from Linux

Hi,i build a yocto and now my goal is to flash the M4 from the yocto system. I tried with echo to the Proc system but geht the following Error. Are there any hint to flash the m4? Is there a better tool for do it?[88303.356298] remoteproc remoteproc0...

Resolved! CCM in stm32mp157

Hi all,If I dedicate the MCU SRAM2 for data and MCU SRAM4 for DMA as shown here, do I get CCM like performance or do I have a risk to have contention on the SRAM2 ?After looking at the bus matrix, I suspect there is no risk but I want to make sure it...

AMART.1 by Associate
  • 1922 Views
  • 2 replies
  • 0 kudos

STPMIC1 - POWER_ON ALTERNATE & MAIN mode

Hi There,When the STPMIC1 goes into POWER_ON ALTERNATE mode via the PWRCTRL pin, does the activation of other Turn-ON condition sources like PONKEY or WAKEUP pins will have a resulting effect to the state of POWER_ON mode? (i.e. also triggers the PMI...

SYEH by Associate II
  • 3288 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.