2020-03-06 12:38 AM
I'd like to connect one USB port to the RTOS, running on the Cortex-M4. According CubeMX this is not possible (no square availble to tick). Is this really not possible?
According the datasheet (DS12505 Rev3, page 19, 'Block Diagram'):
According same datasheet (page 36, 'Bus Matirx'):
This is not clear to me.
Denise
Solved! Go to Solution.
2020-03-06 2:37 AM
Altough using OTG from Cortex-M4 is somewhat possible from pure HW point of view, the SW does not allow this use case due to the fact that USBPHY and all clocks are handled by Linux (including the PLL USB used by both USBH and OTG).
2020-03-06 2:37 AM
Altough using OTG from Cortex-M4 is somewhat possible from pure HW point of view, the SW does not allow this use case due to the fact that USBPHY and all clocks are handled by Linux (including the PLL USB used by both USBH and OTG).
2020-03-06 2:41 AM
Thanks for this clarification. That's a pitty to me, but ok.
Denise
2020-03-06 4:47 AM
You may have to rethink your use case, by e.g. 'subcontracting' the USB data transfer to Linux (e.g. using rpmsg/OpenAMP). For sure system latency and power will not be equivalent than a direct management for M4 (the SRAM size not used by the USB stack could be used to buffer more data locally before requesting Linux<->USB wake up)
2020-03-06 7:16 AM
As 'real-time conditions' are the reason why I want to connect USB to the M4, subcontracting does not really bring a benefit, I think. In my case I assume that using the A7 directly is much simpler. Other solution would be to replace USB by UART to be able to execute everything on the M4.
But thanks for the hint. I will surely investigate to check the rpmsg/OpenAMP feature (it's new to me..)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.