2020-02-28 5:12 PM
I am tring to rebuild kenel for STM32MP157C-DK2 using below url.
After I did 5.4 but it does not work and stop to this point ( root device /dev/mmcblk0p6...).
Let me know how to can rebuild kernel for working.
Thank you.
[ 1.857417] can: netlink gateway (rev 20170425) max_hops=1
[ 1.863493] Key type dns_resolver registered
[ 1.867295] ThumbEE CPU extension supported.
[ 1.871370] Registering SWP/SWPB emulation handler
[ 1.877193] registered taskstats version 1
[ 1.880218] Loading compiled-in X.509 certificates
[ 1.909860] stm32-cpufreq stm32-cpufreq: Failed to get chip info: -517
[ 1.916712] mmci-pl18x 58007000.sdmmc: allocated mmc-pwrseq
[ 1.930026] stm32-cpufreq stm32-cpufreq: Failed to get chip info: -517
[ 1.936906] mmci-pl18x 58007000.sdmmc: allocated mmc-pwrseq
[ 1.942262] stm32_rtc 5c004000.rtc: setting system clock to 2020-02-29 01:00:23 UTC (1582938023)
[ 1.952596] Waiting for root device /dev/mmcblk0p6...
Solved! Go to Solution.
2020-03-05 2:46 AM
The pb was found in the wiki article:
PC $> make ARCH=arm multi_v7_defconfig
should be:
PC $> make ARCH=arm multi_v7_defconfig fragment*.config
The article was updated accordingly. Thanks for pointing this and sorry for the inconvenience !
2020-03-01 7:43 AM
2020-03-01 9:10 AM
I think boot is not contuniuing (there is no code) so there is this problem.
If you can, download newest version on the net.
2020-03-01 3:45 PM
Thanks for info.
Is there more new version than linux-4.19.94.tar.xz ? (I used linux-4.19.94.tar.xz )
2020-03-02 3:08 AM
You can look at this site...
https://linuxlists.cc/l/10/linux-kernel-announce/search/%20Linux%20kernel%205
2020-03-02 11:49 PM
我在使用DK1的时也�?�到这个问题,对比�?程是一致的,目�?怀疑相关的命令有细微的错误。
https://blog.csdn.net/Ambitious_Man/article/details/103699146
�?�以结�?�使用这个网站的命令�?��?程,就能正常�?�动了。
2020-03-03 2:40 AM
Hi,
Issue confirmed - reproduced, investigation ongoing.
Milan
2020-03-05 12:03 AM
Hi all,
Just to double check:
did you well update your DK2 board with the V1.2.0 starter package (before updating the uimage with drm modification) ? I mean reflashing completely your sd card with V1.2.0.
2020-03-05 2:46 AM
The pb was found in the wiki article:
PC $> make ARCH=arm multi_v7_defconfig
should be:
PC $> make ARCH=arm multi_v7_defconfig fragment*.config
The article was updated accordingly. Thanks for pointing this and sorry for the inconvenience !
2020-03-05 7:40 AM
When I try:
PC $> make ARCH=arm multi_v7_defconfig fragment*.config
inside kernel source folder I get:
no matches found: fragment*.config
But, when I execute the command with the right fragment path:
PC $> make ARCH=arm multi_v7_defconfig ../fragment*.config
I get the following errors:
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
YACC scripts/kconfig/zconf.tab.c
LEX scripts/kconfig/zconf.lex.c
HOSTCC scripts/kconfig/zconf.tab.o
HOSTLD scripts/kconfig/conf
#
# configuration written to .config
#
scripts/kconfig/Makefile:109: *** No configuration exists for this target on this architecture. Stop.
Makefile:532: recipe for target '../fragment-03-systemd.config' failed
make[1]: *** [../fragment-03-systemd.config] Error 2
Makefile:286: recipe for target '__build_one_by_one' failed
make: *** [__build_one_by_one] Error 2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.