STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! usage of i2c read command in U-Boot

Hi,I have a custom board with a ST32MP157C and a 24AA025E48 on a i2c bus.In the U-Boot, I want to read the MAC address located in the 24AA025E48 on the i2c bus 1 at address 0x53 at offset 0xFA.When I can use the following commands it works (MAC Addre...

TJann.1 by Associate II
  • 3267 Views
  • 2 replies
  • 0 kudos

Resolved! Mistake in STM32MP1-DK2 schematics?

Hi all.The en.MB1272-DK2-C01_Schematic.pdf states thatARD_A0 : PF14 -> ADC1_IN0ARD_A1 : PF13 -> ADC1_IN1ARD_A2 : ANA0 -> ADC2_IN6ARD_A3 : ANA1 -> ADC2_IN2I've spend quite some time to figure out that this is wrong and the correct pinout is:ARD_A0...

dimtass by Associate II
  • 2145 Views
  • 1 replies
  • 2 kudos

HDMI Input Processor best choice?

Hi, I've been pointed out to STM32 to get a low latency HDMI input (splitted) receiver that can render the input into a video stream and process a neural network on it before sending the computed processed outcome (python or similiar) to another hard...

JBrom.1 by Associate
  • 1891 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.