2020-09-08 2:04 PM
Hi all.
The en.MB1272-DK2-C01_Schematic.pdf states that
ARD_A0 : PF14 -> ADC1_IN0
ARD_A1 : PF13 -> ADC1_IN1
ARD_A2 : ANA0 -> ADC2_IN6
ARD_A3 : ANA1 -> ADC2_IN2
I've spend quite some time to figure out that this is wrong and the correct pinout is:
ARD_A0 : PF14 -> ADC2_IN6
ARD_A1 : PF13 -> ADC2_IN2
ARD_A2 : ANA0 -> ADC1_IN0
ARD_A3 : ANA1 -> ADC1_IN1
Can you please verify and if it's so then update the pdf?
Regards.
Solved! Go to Solution.
2020-09-08 11:26 PM
Hello,
I confirm the discrepancies (which are also present on UM2534).
Update of documents will occur, but not in very short term.
2020-09-08 11:26 PM
Hello,
I confirm the discrepancies (which are also present on UM2534).
Update of documents will occur, but not in very short term.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.