STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Rootfs Size Increasing on Avenger96

Hi,I'm using Avenger96 Board using Build-Sytem through Yocto.I want to increase Rootfs Partition Size to 2Gb.Changes done so far:1)Edited /meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc--ROOTFS_PARTITION_SIZE = "2097152" -...

Resolved! STPMIC1 with LPDDR2 and 3.3VDD

I am designing a board using STM32MP1, STPMIC1A and LPDDR2. I want to use 3.3V VDD not 1.8V as most of peripherals are 3.3V. I am following example in AN5031 Figure 32 LPDDR2 VDD1 is powered from LDO3 in bypass mode which is powered by VDD 1.8V. I pl...

PGE by Associate III
  • 2325 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.