2020-08-26 11:14 PM
Hello everyone, I would like to connect the stm32mp157c-dk2 card with the wm8960 audio codec,here is the device tree configuration I made.
/* sound card*/
snd_i2s2: snd_i2s2 {
compatible = "audio-graph-card";
widgets =
"Microphone", "Mic Jack",
"Line", "Line In",
"Line", "Line Out",
"Speaker", "Speaker",
"Headphone", "Headphone Jack";
routing =
"Headphone Jack", "HP_L",
"Headphone Jack", "HP_R",
"Speaker", "SPK_LP",
"Speaker", "SPK_LN",
"LINPUT1", "Mic Jack",
"LINPUT3", "Mic Jack",
"RINPUT1", "Mic Jack",
"RINPUT2", "Mic Jack";
dais = <&i2s3_port>;
status = "okay";
};
/* i2s3 pin definition */
&pinctrl {
i2s3_pins_a: i2s3-0 {
pins1 {
pinmux = <STM32_PINMUX('E', 12, AF5)>, /* SCK */
<STM32_PINMUX('E', 14, AF5)>; /* SDI */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 13, AF5)>; /* SDO */
bias-disable;
};
};
i2s3_pins_sleep_a:i2s3-1{
pins {
pinmux = <STM32_PINMUX('E', 12, ANALOG)>, /* SCK */
<STM32_PINMUX('E', 13, ANALOG)>, /* SDI */
<STM32_PINMUX('E', 14, ANALOG)>; /* SDO */
};
};
};
/* codec control using i2c5*/
&i2c5 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c5_pins_a>;
pinctrl-1 = <&i2c5_pins_sleep_a>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
status = "okay";
/delete-property/dmas;
/delete-property/dma-names;
// Device tree node for Audio Codec
wm8960: wm8960@1a {
compatible = "wlf,wm8960";
reg = <0x1a>;
AVDD-supply = <&v3v3>;
clocks = <&rcc SPI3>;
clock-names = "mclk";
wlf,shared-lrclk;
codec_port: port@0 {
codec_endpoint: endpoint {
remote-endpoint = <&i2s3_endpoint>;
};
};
};
};
/* audio dai */
&i2s3 {
clocks = <&rcc SPI3>, <&rcc SPI3_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "i2sclk", "x8k", "x11k";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2s3_pins_a>;
pinctrl-1 = <&i2s3_pins_sleep_a>;
status = "okay";
i2s3_port: port {
i2s3_endpoint: endpoint {
remote-endpoint = <&codec_endpoint>;
format = "i2s";
mclk-fs = <256>;
};
};
};I have the following error showing when I try to record audio.
arecord: pcm_read:2143: read error: input/output error
[ 2.215178] st,stm32-i2s 4000c000.audio-controller: No cache defaults, reading back from HW
thank you in advance
2020-08-27 2:34 AM
Hello @l_Homme ,
Could you please confirm that you reworked your board to be able to use IIS from Rpi connector ?
The schematic available in the wiki : Link.
I'am not sure to understand the i2s3 entry in the DT, because I think that codec_endpoint needs to be connected to SAI.
wm8960: wm8960{
[...]
ports {
[...]
wm8960_tx_endpoint: port@0 {
reg = <0>;
remote-endpoint = <&sai2a_endpoint>;
};
wm8960_rx_endpoint: port@1 {
reg = <1>;
remote-endpoint = <&sai2b_endpoint>;
};
};
};And connect them to SAI like the hereafter patch :
sai2a_port: port {
sai2a_endpoint: endpoint {
- remote-endpoint = <&cs42l51_tx_endpoint>;
+ remote-endpoint = <&wm8960_tx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
sai2b_port: port {
sai2b_endpoint: endpoint {
- remote-endpoint = <&cs42l51_rx_endpoint>;
+ remote-endpoint = <&wm8960_rx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};BR,
Christophe
2020-08-27 4:37 AM
thanks for your answer,
however i want to use both codecs, that of the stm32mp1 card (CS42L51) and my new external codec.
so replace the remote-endpoint = <& cs42l51_rx_endpoint>; by remote-endpoint = <& wm8960_rx_endpoint>; don't bother me. you offer me what solution? thank you
2020-09-04 8:50 PM
hello,
Have you solved the problem? I have the same problem as you。
sound: sound {
compatible = "audio-graph-card";
label = "STM32MP1-DK";
widgets =
"Microphone", "Mic Jack",
"Line", "Line In",
"Line", "Line Out",
"Speaker", "Speaker",
"Headphone", "Headphone Jack";
routing =
"Headphone Jack", "HP_L",
"Headphone Jack", "HP_R",
"Speaker", "SPK_LP",
"Speaker", "SPK_LN",
"Speaker", "SPK_RP",
"Speaker", "SPK_RN",
"LINPUT1", "Mic Jack",
"LINPUT3", "Mic Jack",
"RINPUT1", "Mic Jack",
"RINPUT2", "Mic Jack";
dais = <&sai2a_port &sai2b_port &sai4a_port &spdifrx_port &i2s2_port>;
status = "okay";
};
&sai2 {
clocks = <&rcc SAI2>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "x8k", "x11k";
pinctrl-names = "default", "sleep";
pinctrl-0 = <&sai2a_pins_a>, <&sai2b_pins_b>;
pinctrl-1 = <&sai2a_sleep_pins_a>, <&sai2b_sleep_pins_b>;
status = "okay";
sai2a: audio-controller@4400b004 {
#clock-cells = <0>;
dma-names = "tx";
clocks = <&rcc SAI2_K>;
clock-names = "sai_ck";
status = "okay";
sai2a_port: port {
sai2a_endpoint: endpoint {
remote-endpoint = <&wm8960_tx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};
};
sai2b: audio-controller@4400b024 {
dma-names = "rx";
st,sync = <&sai2a 2>;
clocks = <&rcc SAI2_K>, <&sai2a>;
clock-names = "sai_ck", "MCLK";
status = "okay";
sai2b_port: port {
sai2b_endpoint: endpoint {
remote-endpoint = <&wm8960_rx_endpoint>;
format = "i2s";
mclk-fs = <256>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <32>;
};
};
};
};
wm8960: wm8960@1a {
compatible = "wlf,wm8960";
reg = <0x1a>;
#sound-dai-cells = <0>;
status = "okay";
//wlf,shared-lrclk;
wlf,capless;
clocks = <&sai2a>;
clock-names = "MCLK1";
ports {
#address-cells = <1>;
#size-cells = <0>;
wm8960_tx_port: port@0 {
reg = <0>;
wm8960_tx_endpoint: endpoint {
remote-endpoint = <&sai2a_endpoint>;
};
};
wm8960_rx_port: port@1 {
reg = <1>;
wm8960_rx_endpoint: endpoint {
remote-endpoint = <&sai2b_endpoint>;
};
};
};I have the following error showing when I try to record audio.
arecord: pcm_read:2143: read error: input/output error
[ 4.369396] st,stm32-i2s 4000b000.audio-controller: No cache defaults, reading back from HW
2020-09-07 1:20 AM
Hello @l_Homme ,
It's not possible to use the 2 channels of both codecs on Disco board because both codecs share same wires / SAI.
BTY, do you plan to use tx and rx for each codec ?
BR,
Christophe
2020-09-07 1:27 AM
Hello @Christophe Guibout ,
no no I would like to use only the RX for each codec
2020-09-07 2:21 AM
Hello @l_Homme ,
In that case, I would recommend to connect sai2a_endpoint to wm8960_rx_endpoint and sai2b_endpoint to cs42l51_rx_endpoint.
You also need to open/close SB1~SB4 and SB13~SB16 accordingly.
BR,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.