2020-09-04 8:48 AM
Hello,
I have an STM32MP157C-DK2 running OpenSTLinux using the STM32MP1Starter 2.0 image. I am wondering if it is possible to enable spidev drivers such that /dev/spidevx.x devices are available. I see that sys/bus/spi/devices exists, but there is nothing listed under it. I didn't see any spidev packages available using apt-cache search either.
Also, this may or may not be related, but i2c5, which according to https://www.st.com/resource/en/user_manual/dm00591354-discovery-kits-with-stm32mp157-mpus-stmicroelectronics.pdf is what is used on CN2 (the 40-pin header) is not appearing either.
Thanks
Melissa
Solved! Go to Solution.
2020-09-06 10:33 PM
Hi,
for peripherals to be recognised in Linux you need to activate them in the device tree. For a start see here: https://wiki.st.com/stm32mpu/wiki/Device_tree
To specifically enable the spi you can look at this page: https://wiki.st.com/stm32mpu/wiki/SPI_device_tree_configuration
All other peripherals are listed here: https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
To manually compile the device tree you will need the Linux kernel source code and the ST SDK. The device tree file you will want to configure is the stm32mp157c-dk2.dts file, which is the description for the dk2 development board. To compile the device tree take the following steps:
/* source the ST SDK before */
cd <linux source directory>
make stm32_defconfig
make stm32mp157c-dk2.dtbYou will end up getting the compiled device tree in the folder arch/arm/boot/dts/stm32mp157c-dk2.dtb.
Replacing the old device tree (you should find it in the /boot/ directory) on your board should enable the peripherals you activated after a reboot.
For using the spidev this might help you: https://stackoverflow.com/questions/53634892/linux-spidev-why-it-shouldnt-be-directly-in-devicetree
2020-09-06 10:33 PM
Hi,
for peripherals to be recognised in Linux you need to activate them in the device tree. For a start see here: https://wiki.st.com/stm32mpu/wiki/Device_tree
To specifically enable the spi you can look at this page: https://wiki.st.com/stm32mpu/wiki/SPI_device_tree_configuration
All other peripherals are listed here: https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
To manually compile the device tree you will need the Linux kernel source code and the ST SDK. The device tree file you will want to configure is the stm32mp157c-dk2.dts file, which is the description for the dk2 development board. To compile the device tree take the following steps:
/* source the ST SDK before */
cd <linux source directory>
make stm32_defconfig
make stm32mp157c-dk2.dtbYou will end up getting the compiled device tree in the folder arch/arm/boot/dts/stm32mp157c-dk2.dtb.
Replacing the old device tree (you should find it in the /boot/ directory) on your board should enable the peripherals you activated after a reboot.
For using the spidev this might help you: https://stackoverflow.com/questions/53634892/linux-spidev-why-it-shouldnt-be-directly-in-devicetree
2020-09-07 10:37 AM
Thanks, I was just hoping there was a simpler way.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.