STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Alsa no sound card found

Hi All,i'm having an issue with STM32MP157c and audio driver WM8994 (same as used into STM32MP15-DK).At boot time i'm still have the following error:[   4.250237] ALSA device list:[   4.251761]  No soundcards found.I share the electrical drawing of o...

0693W00000FDwlQQAT.png
IDe P.1 by Associate II
  • 4440 Views
  • 4 replies
  • 0 kudos

Resolved! Exit from standby

EDIT: Found the solution, read for implementationI'm trying to get the MPU to exit from standby. PWR_ON goes to 0 as expected on shutdown, so far so good.I'm using PA2 (WKUP2) but it's not working at all...Is there anything special to setup in the de...

fpoussin by Associate III
  • 3166 Views
  • 3 replies
  • 0 kudos

Resolved! Fail to reset from linux

I'm having trouble resetting the board from linux.Not using a PMIC but discrete power supplies.I followed the app notes and errata, connecting the NRST and CORE_NRST pins with a cap then later a 0R resistor.I'm using a single 100nF cap on NRST.I can ...

0693W00000FDZNVQA5.png
fpoussin by Associate III
  • 2675 Views
  • 3 replies
  • 0 kudos

How to configure USART1 on STM32MP157c

Hi All,i have my own board based on STM32MP157C.I connected usart1 (tx, rx, cts, rts) to Wifi/Ble module and i still got the same error:stm32-usart: probe of 5c000000.serial failed with error -22I discovered that USART1 is a secure device so i need t...

IDe P.1 by Associate II
  • 5519 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.