STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I've been looking at the Raspberry Pi for a field IOT application, but I understand that it is not secure ...

I have been told that the STM32MP1 fit that criteria. ie if the board is deployed to the field, then it is not easy to reverse engineer the SD card, ripping code and configuration details.Is this indeed true?What is the equivalent model to the Pi in ...

MTayl.4 by Associate
  • 1181 Views
  • 0 replies
  • 0 kudos

Resolved! OpenSSL performance expectation

I am wondering what number I should expect in terms of encryption performance with STM32MP157C. Below is that I getOpenSSL 1.1.1l 24 Aug 2021 # openssl engine -c (devcrypto) /dev/crypto engine [DES-CBC, DES-EDE3-CBC, AES-128-CBC, AES-192-CBC, AES-2...

CErik.2 by Associate II
  • 3043 Views
  • 3 replies
  • 0 kudos

MicroSD initialization timeout. When inserting the sd card, dmseg shows "mmc0: error -110 whilst initialising SD card" With some logs, i see that mmc_send_app_op_cond is the function that timeouts.

My device tree is the following:&sdmmc1 { pinctrl-names = "default", "opendrain", "sleep"; pinctrl-0 = <&sdmmc1_b4_pins_a>; pinctrl-1 = <&sdmmc1_b4_od_pins_a>; pinctrl-2 = <&sdmmc1_b4_sleep_pins_a>; cd-gpios = <&gpiog 1 (GPIO_ACTIVE_LOW | GPIO_P...

0693W00000FDx2HQAT.png
Lmoio.1 by Senior
  • 3212 Views
  • 4 replies
  • 0 kudos

Warning: Source ID *** was not found when attempting to remove it. I have a question which boards from the STM32MP157 family do not have this problem? Sincerely, Alexander.

Good afternoon, I wrote a program for controlling the railway scoreboard in Python 3 for the STM32MP157A-DK1 board. I have a problem. It is described by the link https://bugs.launchpad.net/ubuntu /+source/gnome-control-center/+bug/1264368Troubleshoot...

Vlaty.1 by Senior
  • 3247 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.