STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install crontab on Stm32mp1? Inside starter package rfs, I found this file /etc/cron.daily/apt.apt-compat.cron.daily but crontab is not present: root@stm32mp1:~# crontab -sh: crontab: not found so the file will never be executed, am i correct?

I can't install crontab with apt-get installapt-get install cron Reading package lists... Done Building dependency tree Reading state information... Done E: Unable to locate package cronWhat do you suggest?

Lmoio.1 by Senior
  • 1731 Views
  • 2 replies
  • 0 kudos

Resolved! Kernel initialization problem - timeouts

Hi,I'm trying to make a custom board boot, using buildroot with all the official ST releases (tf-a, u-boot, kernel) but it's getting blocked at some point.[ 0.911310] stm32mp1_rcc 50000000.rcc: deferred probe timeout, ignoring dependency [ 0.92...

fpoussin by Associate III
  • 5530 Views
  • 6 replies
  • 0 kudos

Issue booting on custom board

I have board based on MB1277 design but on my custom board I'm getting this issue:NOTICE: CPU: STM32MP157AAC Rev.B NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother INFO: Reset reason (0x15): INFO: Power-on Reset (r...

MBeli.1 by Associate III
  • 2975 Views
  • 7 replies
  • 0 kudos

Resolved! stm32-dwmac: Support of multiple VLAN ids

Hi,we have designed a custom board, based on STM32MP151 and OpenSTLinux 5.10. On this board we use the switch NXP SJA1105S with 3 phys and a MAC-MAC interface between the MPU and the switch. All ports are configured for RGMII mode. At startup(via mod...

CHoll.2 by Associate II
  • 5410 Views
  • 6 replies
  • 0 kudos

Resolved! Hello, I'd like to preserve time after rebooting, when no internet connection is present. Every time I reboot I get the same date, which i presume is the late date there was an internet connection. I'd like to update this system clock with the current tim

root@stm32mp1:~# timedatectl status Local time: Thu 2021-10-14 15:10:06 UTC Universal time: Thu 2021-10-14 15:10:06 UTC RTC time: Sat 2000-01-01 00:00:38 Time zone: UTC (UTC, +0000) System cl...

Lmoio.1 by Senior
  • 5003 Views
  • 5 replies
  • 0 kudos

Resolved! WiFi Module choice for STM32MP15

Hi,On the DK2 board, there is a LBEE5KL1DX-883 from Murata. But I want to use their LBEE5HY1MW (Type 1MW - LBEE5HY1MW | Wi-Fi® Modules / Wi-Fi® + Bluetooth® Modules | Murata Manufacturing Co., Ltd.) in my design. But on their site, they only mentions...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.