STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to set the OTP bits?

I have a custom STM32MP157c board. I try to set fuse bits (3 0x23000000). It worked on the basic boot system but not on the TF-A boot system. I mean by example the boot command : fuse prog 0 3 0x23000000.

Ronte.1 by Associate III
  • 7469 Views
  • 7 replies
  • 0 kudos

Question about custom machine

Hi!I am using a STM32MP157C-DK2 board to create an application on the screen. I have used STM32CubeIDE to create my own program:I have initialized peripheral with its default modeI have enabled FDCAN peripheralI have changed the clock settings.With t...

TArre.1 by Associate III
  • 2007 Views
  • 1 replies
  • 0 kudos

STM32MP157F: Dmaengine dmaengine_prep_dma_memcpy vs dmaengine_prep_dma_cyclic? Hardware vs Software triggered. (Linux)

Hello all!​We have implemented our custom driver that uses DMA to copy a large amount of data from the FMC interface (FPGA mapped to it) to the RAM.​For very fast data acquisition the setup time for new DMA transactions becomes critical.I tried an ov...

GLaure by Senior
  • 2584 Views
  • 3 replies
  • 0 kudos

Resolved! “Error: failed to download Segment[0]�? Populate the target and boot the image example

“Error: failed to download Segment[0]�?I looked at the other items with the same title but did not see an answer that would help me.I am using the STM32MP157F-DK2The demo code was working when box was openedI tried to run the demo“Populate the target...

JAmia.1 by Associate II
  • 11470 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.