STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32mp157 Programming NOR flash

Trying to load TF-A and uboot into NOR flash, but I always get this error.SF: Detected w25q256 with page size 256 Bytes, erase size 64 KiB, total 32 MiBmtdids=nor0=nor0 & mtdparts=mtdparts=nor0:256k(fsbl1),256k(fsbl2),2m(ssbl),512k(u-boot-env),-(nor_...

uouox by Associate II
  • 2454 Views
  • 2 replies
  • 0 kudos

Issues while programming board STM32MP157C-dk2 over STM32CubeProgrammer. See details below.

STM32MP157C-dk2I am trying to update the Board using SUART3 (Pins PB10, PB12) over STM32CubeProgrammer. The connection to STM32CubeProgrammer is established successfully. Unfortently after downloading the fdbl-boot (tf-a-stm32mp157c-dk2-uart.stm32) t...

WSief.1 by Associate II
  • 3559 Views
  • 5 replies
  • 0 kudos

Failed to access ROM Table of CortexM4 while debugging in engineering mode. What are the reasons ? See description below.

Product: STM32MP153CAA3we are trying to debug the Cortex M4 over the SWD Interface. The setup of the Bank0,1,2 is configured correct (Engineering Mode) . During the analysis of SWD we see that Debugger fails to access ROM Table (Address: 0xE00FFFE4, ...

WSief.1 by Associate II
  • 2468 Views
  • 3 replies
  • 1 kudos

LCD not interpreting colors correctly using LTDC connected to STM32MP157F based custom board.

We have a custom board based on STM32MP157 MPU and running AOSP, with AUO G101EVN010 LCD-TFT panel using an LVDS to LTDC converter for interface.Setup of the system is done using the STM32MP1 distribution for Android. I am able to get the panel to di...

_legacyfs_online_stmicro_images_0693W00000bkDBHQA2.png _legacyfs_online_stmicro_images_0693W00000bkDDDQA2.png
SRaic.1 by Associate II
  • 1474 Views
  • 0 replies
  • 0 kudos

Resolved! Configuring and reading "GPIO Analog"

Using the STM32MP157 development kit, I have configured two "GPIO Analog" lines that are exposed through CN13 (pins 1 and 2).I am trying to set these up as such. From going down the rabbit trail of documentation:https://wiki.st.com/stm32mpu/wiki/GPI...

_legacyfs_online_stmicro_images_0693W00000bk7OZQAY.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.